2018-11-29 2:41 AM
Hi,
I use my device for continuous scanning. The scanning is started by calling:
aci_gap_start_general_discovery_proc(
2000 /*LE_Scan_Interval = 1.25 s */,
1800 /*LE_Scan_Window = 1.125 s */,
0x00 /*=use public dev addr */,
0x00 /*=duplicate filtering dissabled*/);After 10 seconds, this procedure automatically terminates, and this is signalled by the event:
aci_gap_proc_complete_event(...)
with arg. Procedure_Code == 0x02 /*= GENERAL_DISCOVERY_PROC*/I detect it and re-enable discovery procedure. While discovery procedure is working I receive correct ADV_IND (reports) from sensor devices.
This regular behaviour and works fine.
Unfortunatelly, sometimes I do not receive the event. No advertisement reports are received then.
When it happens I cannot terminate the discovery procedury nor start it again. Both functions: aci_gap_start_general_discovery_proc, aci_gap_terminate_gap_proc(0x02) return the error: 12 ERR_COMMAND_DISALLOWED.
Why the event is missing?
Regards,
Piotr
PS
I use BlueNRG-2 in network processor communication mode. It is connected via SPI with STM32 where is my application. BlueNRG-2 is programmed with DTM firmware. I use DK-3.0.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.