Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can the BlueNRG-2 chip be programmed through SWD?

I have the STEVAL-IDB008V2 board, and it programs decently through the ST-Link V2. However, I am facing troubles with programming the BlueNRG-2 chip through SWD of another Disco board. Can anyone please tell me whether the BlueNRG-2 can be programmed...

abbas14 by Associate II
  • 607 Views
  • 0 replies
  • 0 kudos

Sending At Commands to SPBT3.0DP2 via mbed

I am trying to use mbed to send AT Commands to the SPBT3.0DP2 module in order to change it's baud rate. I am using the ATCmdParser to send the AT commands. It seems like I am not able to enter the command mode? I'm not sure. please help.I do at.send(...

JMin.17 by Associate II
  • 983 Views
  • 0 replies
  • 0 kudos

Error message "Could not initialize BlueNRG Mesh library!", error code = 2 when using pre-built bin file for NUCLEO-L476RG with X-NUCLEO-IDB05A1

I also built firmware from provided sources and libraries using WorkBench but the problem persisted. One thing was different, bin file was less than half the size of the pre-built one. I added some code to display returned error code (2) and also dis...

Boris3 by Associate
  • 1074 Views
  • 1 replies
  • 0 kudos

ST7580 transmitter/receiver circuit question

In the ST7580 application note (AN4068) the transmitter and receiver paths are connected through a DC blocking capacitor after the output of the power amplifier. Therefore when no transmission is occurring the output of the PA should be similar to a ...

LSmit.10 by Associate
  • 734 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.