2021-09-02 5:33 AM
Hello,
I'm using Nucleo l4r5zi-p in which I configured the USB device CDC. When I transmit data using the CDC_Transmit_FS function some time it returns USBD_BUSY, sometimes USBD_OK so because of USBD_BUSY I'm not getting actual speed. But I'm transmitting continuous data then why does it return USBD_BUSY?
Thanks,
Yash
2021-09-13 3:15 AM
Hello @Yash ,
It is normal to get the USBD_BUSY status when transmitting data. Could you please provide more details ?
As well, What do you mean by "I'm not getting actual speed" ?
Otherwise, you can refer to the following example : (Path: Projects\STM32L476G-EVAL\Applications\USB_Device\CDC_Standalone )
I hope this help you.
BeST Regards,
Walid
2021-09-13 11:04 PM
Hello Walid,
As per USB CDC configuration, the actual speed is 12Mbit/sec but we got around 360 microseconds per byte. But it should be 0.6 microseconds if the USB is working on 12Mbit/sec.
Regards,
Yash
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.