2015-09-28 2:32 AM
Goodmorning,
We bought the STEVAL-IDW001V1 evaluation board and the STEVAL-PCC018V1 module to connect it to the pc; the STEVAL-IDW001V1 it's already updated to the last release FW 3.4.We need to receive some data from a smartphone on a microcontroller connected to the wifi module, the SPWF01SA shall be the server and it shall create a local network to which any smartphone (IOS, Android, Windows) can connect.The SPWF01SA should open a socket (UDP or TCP) on a port already defined and by our app the smartphone should send data to the module.The SPWF01SA should in turn send this data (max 10 byte) to the microcontroller via UART. The smartphone should recognize the network, connect to it, open the tansmission and send data.Is there a SPWF01SA configuration to do this? Is there also an example of instruction which will make thi configuration easier to me? #spwf01sa212015-09-28 7:36 AM
Ciao Fabrizio,
1 - Configure SPWF as a miniAP (e.g., keep pushed SW2 onSTEVAL-IDW001
@ startup);2 - The use your smartphone to join the miniAP network (called ''iwm_xx-xx-xx'');3 - Use a browser to request the ''output_demo.html'' webpage from internal webserver4 - Push data!As an alternative, open a socket server on miniAP (AT+S.SOCKD) on port 80 (to use the browser on the smartphone) or another generic port (in this case, download an App for Android/iOS to open a socket client from the smartphone)Hope to be clearciaojerry2015-10-04 11:40 PM
Hai fabrizio,
I am now working on the same type of project what you posted here but i am using STM32F7 with SPWF01S . The process of communication is same,1. sending data from mobile to SPWF01S2.then from SPWF01S to microcontroller via UART3. micontroller should reply back through UART.Did u find the answer ?If so can you give me some idea to approach?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.