Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flow control not working as I expect

Posted on October 06, 2015 at 16:31 Next problem... I have enabled flow control on the module and the MCU and now attempting to use a bit rate of 460800. Both ends are using the right bit rate but only the MCU appears to be controlling an RTS signal...

markb by Associate II
  • 5170 Views
  • 25 replies
  • 0 kudos

Data Mode SPWF01SC.11

Posted on October 19, 2015 at 16:54Hai Guys !I am using SPWF01SC.11 , I have connected this with the micro controller via UART.From the micro controller I am sending a command AT+S.SOCKD= port number through UART.Now my WiFi module received the comm...

Nandy K by Associate II
  • 1138 Views
  • 2 replies
  • 0 kudos

Cannot connect with AP

Posted on October 11, 2015 at 15:14Hi everybody, I have troubles to connect the SPWF01 with an AP using WPA2 privacy mode. When I try to connect, after Wind 25: association successful, I receive Wind 40: deauthentication:1 +WIND:19:WiFi Join:00:04:E...

paolo23 by Associate II
  • 3454 Views
  • 11 replies
  • 0 kudos

BlueNRG: does it support Prepare Write reception?

Posted on October 09, 2015 at 12:31Hello, we have to transfer long attributes (images) on BlueTooth. We read in BLE Specifications 4.0 that this can be accomplished using the “Write Long Characteristic Values�? procedure described in 4.9.4 of part ...

dario2 by Associate III
  • 815 Views
  • 0 replies
  • 0 kudos

SPWF01 Repeatable Hard Fault/crash

Posted on October 01, 2015 at 09:51Hi, I am broadcasting a small UDP packet once a second through the SPWF01 using AT+S.SOCKON=192.168.1.255,55555,u and AT+S.SOCKW and that appears to work just fine but if I access the SPWF01 web server at the same...

markb by Associate II
  • 4707 Views
  • 14 replies
  • 0 kudos

BlueNRG – Send/Receive Data.

Posted on October 05, 2015 at 11:21 My device is configured as a SERVER in an advertising mode. ret = aci_gap_set_discoverable(ADV_NONCONN_IND, 160, 160, PUBLIC_ADDR, NO_WHITE_LIST_USE, sizeof(local_name), local_name, 0, NULL, 0, 0); ...

BLUENRG - Beacon mode.

Posted on October 01, 2015 at 14:45 First I configure the module. void BLUENRG_Setup(void) { HCI_Init(); BlueNRG_RST(); Osal_MemCpy(bdaddr, SERVER_BDADDR, sizeof(SERVER_BDADDR)); /* Configure BlueNRG address as public (its public addr...

Communication between Stm32F7 and SPWF01S module

Posted on October 01, 2015 at 12:44Hai,I have configured SPWF01S wifi module as miniAP andI have connected STM32F7-Disco with SPWF01S through UART.I am sending the command AT+S.SOCKD = <port number> to the wifi module and it is ready for listening.N...

Nandy K by Associate II
  • 2103 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.