2024-06-13 6:02 AM
Hi,
during maximum heating tests of our device, we measured a case temperature of +92 °C on the STKNX (on top of the plastic package via thermocouple). The environmental temperature near the STKNX and the PCB was +85 °C.
On the borderline, but ok in my opinion.
To make things easier, is there perhaps a maximum value for the STKNX case temperature?
Datasheet information:
TJ = Maximum operating junction temperature = +110 °C
TAMB = Operating ambient temperature = -40 to +85 °C
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.