Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 respond with address 0x7E

Hello Everyone,I am working on a product and recently due to chip shortage I have to change the IMU. I have selected LSM6DS. My MCU is Esp32. now when I send a query of I2C address it responds with 0x7E address while it should be 0x6A. I was using Ad...

0693W00000JN1spQAD.png
Waqas1 by Associate
  • 2537 Views
  • 2 replies
  • 1 kudos

Resolved! STPM33/34 MISO & Insulating barrier

Hello everyone I am looking into the STPM33/34. I only want to use 1 SPI bus for both ICs and select it with the SCS. In the datasheet I cannot see whether the MISO goes into tristate when the IC in question is not active. I also cannot see any infor...

Martin68 by Associate II
  • 7471 Views
  • 12 replies
  • 2 kudos

I need help for ST WiSE Studio

After creating new project in ST WiSE Studio the created folders and files are like in pictureWhen new project is compared with other projects from examplesit is noticed that some folders are missing.One of missing folder is User. In that folder the ...

MTole_0-1717586050887.png MTole_1-1717586303051.png
MTole by Associate II
  • 947 Views
  • 0 replies
  • 0 kudos

BlueNRG-2, Whitelist and Advertising

Hej Folks,I have an application with multiple BlueNRG-2s. There are 1 Master and up to 5 Slaves. I would like to connect the master to these 5 Slaves only, so no other device can connect to them and vice versa. I thought about using a whitelist. Curr...

Yoschii by Associate
  • 1162 Views
  • 0 replies
  • 0 kudos

BlueNRG-2 is detected but cannot be connected.

I am developing software that uses BlueNRG-2 as a peripheral to communicate with a central device.(With reference to BlueNRG-1, BlueNRG-2 BLE stack v2.x programming guidelines(PM0257))I checked using the iPhone (LightBlue app) and it was able to dete...

snwatana by Associate
  • 850 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.