2018-03-19 3:41 AM
I'm trying eval board with SPBTLE-1S module. I'm using BlueNRG-1 Navigator v 2.6.0. If I flash any demo application, no BLE service can be discovered on the phone (Nexus 5X, Android 7.1.1.)
E.g. BLE Sensor demo - DL3 shorty blinks after reset, then BL1 slightly flashes, so the chip is doing something, but no RF signal. (Previous chip TI CC2540 has communicated correctly, with the same phone.)
Have I missed something or is the chip broken?
Solved! Go to Solution.
2018-03-20 6:44 AM
Hi Tomas,
please notice that all the examples included in the
BlueNRG-1 Navigator v 2.6.0 are preconfigured for the
STEVAL-IDB007V1board. In your case, instead, you're using anSTEVAL-IDB007V1M, which needs a different configuration. Indeed, your board is based on the
SPBTLE-1S module, which has a 32 MHz crystal. All the examples that you have found for BlueNRG-1 are usually configured for a 16 MHz crystal (the one used in the EVAL-IDB007V1 board).In order to test the examples with STEVAL-IDB007V1M, you have to rebuild them for 32 MHz. Please make sure that in your project settings you define this:
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
For more information, you can also follow this thread about
https://community.st.com/0D50X00009XkWquSAF
.Best regards,
Antonio
2018-03-20 6:44 AM
Hi Tomas,
please notice that all the examples included in the
BlueNRG-1 Navigator v 2.6.0 are preconfigured for the
STEVAL-IDB007V1board. In your case, instead, you're using anSTEVAL-IDB007V1M, which needs a different configuration. Indeed, your board is based on the
SPBTLE-1S module, which has a 32 MHz crystal. All the examples that you have found for BlueNRG-1 are usually configured for a 16 MHz crystal (the one used in the EVAL-IDB007V1 board).In order to test the examples with STEVAL-IDB007V1M, you have to rebuild them for 32 MHz. Please make sure that in your project settings you define this:
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
For more information, you can also follow this thread about
https://community.st.com/0D50X00009XkWquSAF
.Best regards,
Antonio
2018-03-20 8:40 AM
Hi Antonio,
I have already found that thread (not before, otherwise I shouldn't have written the post), and, if I understand it correctly, it is impossible to make any example working without rebuild, using BlueNRG Navigator only?
I don't have any supported IDE (we are using Rowley Crossworks) and I would like first to try some (ready made!) example before I dig into the project and convert it to our IDE.
Could you please send me the BLE_SensorDemo.hex, compiled for 32MHz Xtal, as you did for Wolfgang?
I was very near to send the board back to the seller as broken piece.
Best regards,
Tomas
2018-03-20 9:45 AM
Hi Tomas,
here is the BLE_SensorDemo.hex file, compiled for 32MHz Xtal.
Please let me know if this works for you, as I don't have any STEVAL-IDB007V1Mto test it myself.
Best regards,
Antonio
________________ Attachments : BLE_SensorDemo.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxpi&d=%2Fa%2F0X0000000b1e%2F5umDH.4WfZUBH8usQuNnMtd05rhXlKJCq3NMan0pF.k&asPdf=false2018-03-21 3:47 AM
Hi Antonio,
Great! Works as expected, many thanks.
It's a pity the original binaries are for this version useless :-((
Best regards,
Tomas
2018-03-21 9:19 AM
Hi Tomas,
I think it would be useful to also add the binaries for the SPBTLE-1S module and the STEVAL-IDB007V1M board. I'll take a note and see if we can add them to the next release of the software package.
Thanks for your feedback,
Antonio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.