2026-05-20 4:51 PM - last edited on 2026-05-22 3:07 AM by Andrew Neil
Hello,
I am testing FP-SNS-BLEMESH1 on two STEVAL-MKBOXPROA boards.
Setup:
Board: STEVAL-MKBOXPRO A
Firmware: BlueNRG-Mesh Sensor Demo v2.1.3
Library: BlueNRG-Mesh Library v01.14.000
Bearer: PB-ADV
One board configured as Embedded Provisioner
One board configured as Sensor Node (unprovisioned device)
The provisioner starts scanning correctly, but no unprovisioned device is found.
At scan step, the console reports that no unprovisioned device is nearby, even when the second board is physically next to the provisioner.
The sensor node logs show:
DIAG: PB_ADV_SUPPORTED=1 PB_GATT_SUPPORTED=1 BEARER_INFO=3 Unprovisioned device BlueNRG-Mesh Sensor Demo v2.1.3 BlueNRG-Mesh Library v01.14.000 BLE Stack Initialized & Device Configured
So the node appears to advertise correctly as unprovisioned.
Since Embedded Provisioner could not discover the node, I switched to the ST BLE Mesh mobile application.
With the mobile app:
the node is detected correctly,
provisioning starts,
provisioning appears to succeed,
Logs:
ATT mtu exchanged with value = 247 Appli_BleUnprovisionedIdentifyCb - Unprovisioned Node Identifier received: 0a BluenrgMesh_ProvisionCallback - Device is provisioned by provisioner
After the message:
BluenrgMesh_ProvisionCallback - Device is provisioned by provisioner
nothing else is printed for some time
At this point:
the mobile application never completes mesh configuration,
the node does not become operational,
the configuration phase appears stuck or crashes immediately after provisioning.
Additional notes:
I tested the official ST binary as well.
Same behavior occurs with the official firmware.
PB-ADV was used.
Two official STEVAL-MKBOXPRO boards were used.
Questions:
Is Embedded Provisioner mode fully supported and validated on STEVAL-MKBOXPRO in FP-SNS-BLEMESH1 v2.1.3?
Are there known issues where unprovisioned beacons are not detected by the Embedded Provisioner scan module in this firmware version?
Why does the ST BLE Mesh app stop after provisioning success callback without completing node configuration? Is there a recommended configuration for stable provisioning/configuration on SensorTile.box PRO?
Thank you.
2026-05-22 3:00 AM
Did you configure the mesh nodes manually before testing, or did you only flash both STEVAL-MKBOXPROA boards directly with FP-SNS-BLEMESH1 default firmware? and how ?I am asking because using the default firmware directly on both boards might explain why the Embedded Provisioner cannot discover the unprovisioned node or why provisioning/configuration stops after the provision callback.
2026-05-22 4:19 AM
Both boards were flashed with custom firmware based on FP-SNS-BLEMESH1 v2.1.3, not the default binary. The configuration was done explicitly:
Board 1 (Embedded Provisioner):
Board 2 (Sensor Node):
The core issue on Issue #1 is that BluenrgMesh_GetNeighborState() always returns 0 entries on BlueNRG-LP, even with the node physically adjacent. We confirmed through HCI callback instrumentation (hci_le_advertising_report_event override) that zero advertising reports are received by the provisioner, despite the sensor node broadcasting correctly. This points to a known BlueNRG-LP limitation where ADV_NONCONN_IND packets are not surfaced unless aci_gap_start_procedure(GAP_OBSERVATION_PROC) is called explicitly — but calling it manually conflicts with the mesh library's internal scan state machine.
On Issue #2, provisioning via ST BLE Mesh app succeeds (NVM persists Provisioned node across reboot), but the configuration phase (AppKey Add, Model Bind, Publication Set) never completes. I observed the same behavior with the official ST binary, ruling out a firmware customization issue.
2026-05-22 5:31 AM
it might be because the OOB ( static) tell me how you configured ( what you modified in the code ) exactly and i will correct it with you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.