2017-07-17 10:04 AM
Hi all,
Following the schematics for the
and the schematics for the where the LEDs are connecting from the pins to ground. There is a new schematic () that I have just encountered that has these said LEDs are connecting to the pins from a 3.3V source. Which one of these schematics are correct?I am having the issue where the LINK LED goes off after it makes a successful link. This does not seem to be correct and it would seem that the link LED should light up once a successful link occurs.
It would seem that the new schematic(
STEVAL-3DP001V1)
has the LEDs correct.Any insight into this issue would be greatly appreciated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.