2025-06-10 5:01 AM
Hello,
Could you please provide a simple example source code to operate an S2-LP transceiver under the following conditions? My MCU is an STM32F103 connected via SPI1.
A 25 MHz crystal is fitted to the S2-LP.
External SMPS (1.8 V) is used.
I want to transmit at 420 MHz with 0 dBm output power.
Data rate is 10 kbps, using 2-GFSK modulation with 20 kHz frequency deviation.
Payload is any 20 bytes of data.
Thank you!
2025-06-11 1:09 AM
Have you looked on the 'Tools & Software' tab of the Product Page:
https://www.st.com/en/wireless-connectivity/s2-lp.html#tools-software
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.