2022-07-13 11:22 PM
Hi All,
I want to ask "is it possible to run BLUENRG-355 on internal oscillator (64Mhz) "
As per data sheet it supports internal HSI but device firmware says HSE only.
/* High speed crystal configuration: BlueNRG-LP supports only HSE 32 MHz */
SystemTimer_TimeoutConfig(32000000, 100, TRUE);
2022-07-19 8:59 AM
Hello,
I do confirm an external 32MHz xtal and use of HSE is mandatory.
Regards
Laurent
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.