2020-05-05 12:08 PM
Hi
I am looking to used X-Nucleo-IDB05A2 board for BLE development.
After reading about the information provided on the board page the only example project folder I got, i.e en.x-cube-ble2
After going through all the project given in the folder I didn't got any firmware code for X-nucleo-IDB05A2, only I can see the reference code for X-nucleo-IDB05A1 and X-nucleo-IDB04A1.
So can I use same library as for X-nucleo-IDB05A1 or any changes required?
2020-05-06 5:58 AM
Hi,
yes, please use the same library.
An update of the X-CUBE-BLE1 package will be coming in the near term.
BR
Silvio
2020-05-08 12:50 AM
Hi Silvio,
Thank you for the ans.
I have one more doubt
Can I use FP-AUD-BVLINK1 project library for the same board?
2020-11-19 9:31 AM
Hi,
i have x-nucleo-idb05a2 with STM32F401RE-Nucleo Rev C.
I have put all Binary Application of X-CUBE_BLE1 but never see Bluetooth from scan or from ST BLE Profile.
Why?
2022-07-17 7:47 AM
is this update available yet?
2022-07-18 1:19 AM
2022-07-18 1:58 AM
Thanks.
Is it correct that X-CUBE-BLE2 is incompatible with the X-nucleo-IDB05A2?
It would be (very) nice if the product page would explicitly define which version of a certain package is compatible.
It is also unclear to me which ACI version is supported by this X-nucleo-IDB05A2.
And the correct document that outlines how to configure the X-CUBE-BLE1 package is very hard to find.
Thanks
2022-07-18 2:19 AM
Hello,
the sw package for the X-NUCLEO-IDB05A2 is the X-CUBE-BLE1.
This information is reported in the Overview tab of the X-CUBE-BLE1 page. While, in the Tools & Software tab of the X-NUCLEO-IDB05A2 page, you can find the reference to the X-CUBE package for this board.
In the X-CUBE-BLE1 page (at the bottom), along with the documentation, you can find also the link to the Getting Started with X-CUBE-BLE1 video showing how to use the package with the STM32CubeMX tool.
BR
Silvio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.