2020-10-29 4:24 AM
Pin connection:
ST link ------ BLUENRG232
SWDIO SWDIO
SWCLK SWCLK
GND GND
3.3V VCC
I have also made IO7 high with 10K resister To GND.
Pls. help me out.
2020-10-29 4:37 AM
Hi,
could you please detail a bit more your setup and needs?
If you need to update the BlueNRG-2 module firmware of X-NUCLEO-BNRG2A1, we would suggest to refer to the procedure reported in section 1.2.2 of this guide.
Hope this can help.
Kind regards
2020-10-29 5:22 AM
hi
all i need help is
I have not buy any board of your BLUENRG evaluation board.
I am using IC and supporting Circuit.
My Problem is that can you tell me what changes I have to do with software or hardware to make it run.
2020-10-29 5:29 AM
I will make you understandable through this.
I have BLUENRG232 IC (https://www.digikey.in/product-detail/en/stmicro/BLUENRG-232/497-17582-1-ND/7565506?cur=INR&lang=en&utm_adgroup=RF%2FIF%20and%20RFID&utm_source=google&utm_medium=cpc&utm_campaign=Smart%20Shopping_Product_RF%2FIF%20and%20RFID&utm_term=&productid=7565506&gclid=CjwKCAjw0On8BRAgEiwAincsHAUyGWwc01w4edFI8TV9pMPrf-0No1wSfc2aASG-95pkZ7K0-41JhBoCi5IQAvD_BwE)
Tell me its supporting circuit and how to upload code to it and debug using BLUENRG1_ST_LINK_UTILITY ?
2020-10-29 6:34 AM
2020-10-29 10:32 AM
I am having the same problem. I made PCB with supporting circuit for BLUENRG. The St link utility is not detecting the target.
2020-10-29 10:37 AM
please share the setting we need to make for target in BLUENRG ST link utility
2020-10-29 7:44 PM
look I tell you what I understand,
I have to connect IO7 to GND(and other pins of course) and it should work.
but even though its not working.
Can you read the datasheet and tell me what I am doing wrong?
should I have to connect some other components to IC to make it work?
2020-10-29 7:56 PM
What I Have to do make IO7 high or low?
These are both from section 3.23 of your datasheet(first tell me difference btw. them and then solution):
Regards
2020-10-30 2:16 AM
I gone through the section 3.21 of this Datasheet reports the SWD debug feature. But sill not resolved the issue. Please help me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.