Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Usb Type C

Hi,We would like to use USB Type C PD chip for Data role or Power role swap functionality.We are designing the android accessory using type c connector.We would like to keep our accessory in Device mode and also want to do the charging of smartphone ...

PVala.1 by Associate II
  • 616 Views
  • 0 replies
  • 0 kudos

ST E EV C518 and ST E EV C612 The board stopped working after a power surge, how to fix it? How to replace these elements? The inscriptions are! ST E EV C518 and ST E EV C612

Comrades, tell me, what is this element on the board?The board stopped working after a power surge, how to fix it? How to replace these elements?The inscriptions are!ST EEVC518andST EEVC612

AAlex.11 by Associate
  • 2400 Views
  • 1 replies
  • 0 kudos

I have configured my Bluenrg2 with the help of Bluenrgsdk module with Data Length Extension of 251 bytes and ATT_MTU as 247 and I have acheived a throughput speed around 300kbps but range is the main problem,it gets disconnected if i go beyond 3meters.

I am using BLE_Throughtput_Ext program from Bluenrgsdk version 3.1.0.I have also configured Tx power levels from -14dbm to 8dbm and the results are same(I can see very small variation in my distance of around 2m) as the distance increases my data rat...

KV.271 by Associate
  • 670 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.