2019-05-31 11:48 AM
I have a custom primary service (in server role) with a R/W characteristic set for 27 bytes of data and GATT_NOTIFY_WRITE_REQ event mask. My android client app is sending a verified 27 byte payload to this characteristic. I only get events with 20 byte data length and only the first 20 bytes of the payload in the data buffer. hci_read_buffer_size returns 27 bytes as the packet length. HOW do I obtain the full 27 byte payload??
2019-06-02 10:59 PM
Do you see 1 or 2 write requests?
Maybe the GATT write request is fragmented into 2 packets (L2CAP fragmentations) -
the first one has 23 bytes ATT PDU (3-byte opcode + 20-byte data), and the second has 7-byte ATT PDU.
Please try to use ACI_GATT_ATTRIBUTE_MODIFIED_EVENT event instead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.