Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
I have a custom primary service (in server role) with a R/W characteristic set for 27 bytes of data and GATT_NOTIFY_WRITE_REQ event mask. My android client app is sending a verified 27 byte payload to this characteristic. I only get events with 20 ...
I have a custom primary service (in server role) with a R/W characteristic set for 27 bytes of data and GATT_NOTIFY_WRITE_REQ event mask. My android client app is sending a verified 27 byte payload to this characteristic. I only get events with 20 by...
Good afternoon eveyoneWe want to replace the conventional capacitive touch screen with a resistive touch screen. Capacitive touch screens do not require calibration, but resistive touch screens require a first calibration. I know there is a touch c...
Hello, I am using stm32F429zi as TCP server just like in the example project "echo server" and my application needs to responding every time on the same port, but after disconnect and connect to the sever it changes port. Is there any way to force re...
Discover 2 ways to customize STUSB4500 behavior to meet specific application needs
I am trying to implement a working MESH network without the participation of a smartphone. The idea is to send messages from all test nodes to one specific node through the MESH, which has the same hardware structure as the rest. This node should pro...
I am using a B-L072Z-LRWAN1 and the STM32CubeExpansion_LRWAN_V1.2.1 End node example with an 8 channel lora gateway set to channels 1-8. The gateway is receiving some data from the End Node. Appears the End Node may be transmitting on channels that t...
Posted on January 07, 2018 at 03:35 Hi I have my custom RF board using S2-LP and balunBALF-SPI2-01D3 ( /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fdatasheet%2Fgroup3%2Fe9%2Fff%2Fcd%2F1e%2F4...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.