2018-09-11 4:40 AM
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_SPI3_Init();
MX_USART1_UART_Init();
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
osKernelStart();
while (1) {
}
}
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_SPI3_Init();
MX_USART1_UART_Init();
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
osKernelStart();
while (1) {
}
}
/* USER CODE BEGIN 4 */
static void Echo_TCP(void) {
struct netconn *connection, *newconnection;
err_t err, accept_err;
struct netbuf* buffer;
void* data;
u16_t len;
err_t recv_err;
//Makro tworzące nową strukturę oraz inuicjalizyjące ją nowymi wartościami.
connection = netconn_new(NETCONN_TCP);
if (connection != NULL) {
err = netconn_bind(connection, NULL, 6610); //Przypisz połączenie do portu 6610
if (err == ERR_OK) {
netconn_listen(connection); //Połączenie zamienione na tryb słuchania
while (1) {
//Funkcja oczekujaca na polaczenie od klienta
accept_err = netconn_accept(connection, &newconnection);
//Obsluga polaczenia
if (accept_err == ERR_OK) {
while ((recv_err = netconn_recv(newconnection, &buffer))
== ERR_OK) {
do {
netbuf_data(buffer, &data, &len);
HAL_GPIO_TogglePin(PK_1_GPIO_Port, PK_1_Pin);
netconn_write(newconnection, data, len, NETCONN_COPY);
} while (netbuf_next(buffer) >= 0);
netbuf_delete(buffer);
}
//Zamknij polaczenie
netconn_close(newconnection);
netconn_delete(newconnection);
}
osDelay(10);
}
} else {
netconn_delete(newconnection);
} //Nie udalo się nawiazac polaczenia
}
}
static void Echo_UDP(void){
struct netconn *connection;
struct netbuf* buffer;
static ip_addr_t *addr;
static unsigned short port;
char bufor[100];
err_t err;
connection = netconn_new(NETCONN_UDP);
if(connection != NULL){
err = netconn_bind(connection, NULL, 5109);
if(err == ERR_OK){
while(1){
err = netconn_recv(connection, &buffer);
if(err == ERR_OK){
addr = netbuf_fromaddr(buffer);
port = netbuf_fromport(buffer);
netconn_connect(connection, addr, port);
netbuf_copy(buffer, bufor, buffer->p->tot_len);
bufor[buffer->p->tot_len] = '\0';
netconn_send(connection, buffer);
netbuf_delete(buffer);
}
osDelay(10);
}
}
}
}
/* USER CODE END 4 */
/* StartDefaultTask function */
void StartDefaultTask(void const * argument)
{
/* init code for LWIP */
MX_LWIP_Init();
/* USER CODE BEGIN 5 */
// Echo_TCP();
// Echo_UDP();
/* definition and creation of taskTCP */
osThreadDef(taskTCP, taskTCP_Start, osPriorityNormal, 0, 128);
taskTCPHandle = osThreadCreate(osThread(taskTCP), NULL);
/* definition and creation of taskUDP */
osThreadDef(taskUDP, taskUDP_Start, osPriorityNormal, 0, 128);
taskUDPHandle = osThreadCreate(osThread(taskUDP), NULL);
// vTaskDelete(defaultTaskHandle);
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END 5 */
}
/* taskTCP_Start function */
void taskTCP_Start(void const * argument)
{
/* USER CODE BEGIN taskTCP_Start */
Echo_TCP();
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END taskTCP_Start */
}
/* taskUDP_Start function */
void taskUDP_Start(void const * argument)
{
/* USER CODE BEGIN taskUDP_Start */
Echo_UDP();
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END taskUDP_Start */
}
2018-09-13 8:09 PM
Maybe increase the MEMP_NUM_NETCONN definition in LwIP ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.