Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-MS / SPBTLE-RF Tx power

Hello,​The data sheet for BlueNRG-MS specifies the tx power from -18 dBm to +8 dBm. However, the data sheet from SPBTLE-RF, which embeds the BlueNRG-MS, specifies the maximum tx power as +4 dBm. Where does the 4 dB loss come from? Does this mean, tha...

Hello ! I am trying to start an echo server, parallel to TCP and UDP. When I start them separately - it works. When two separate threads are started - TCP immediately rejects connections and UDP does not respond. How should I do it?

int main(void) { /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init();   SystemClock_Config();   MX_GPIO_Init(); MX_I2C1_Init(); MX_SPI3_Init(); MX_USART1_UART_Init();   osThreadDef(defaultTask,...

TDrzy by Associate II
  • 1343 Views
  • 1 replies
  • 0 kudos

can STEVAL-ILL083V1 board with stm32-L051K6 and SPBTLE-1S can be implemented in mesh technology and how ??

I am using the board STEVAL-ILL083V1 for controlling street light i.e. on/off/dimming. According to the given package it can be performed for individual board. Now I am thinking of to treat STEVAL-ILL083V1 as a node and want to take several such node...

ARAMP by Associate II
  • 948 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.