2018-11-20 9:26 AM
I have an nRF52 DK and a CR95HF development board from Mikroe (https://www.mikroe.com/rfid-click) and I'm using the Nordic SPI SDK version 14.2.0
I have managed to get the device to communicate with the CR95HF and got through the calibration phase, where at each step it correctly responds to the requests.
I am developing on Linux.
However, after sending REQA, to which it responds correctly for my MIFARE Classic card that I'm using as a test device.
I then have to send Anti-Collison, to which it doesn't respond and only after sending many of these same requests repeatedly do I get an 0x81 response.
The only other response I've gotten is 0x82 which is "invalid protocol" per CR95HF documentation.
The reqa request and anti-collision look as follows:
/* REQA from tag */
uint8_t m_txreqa_buf[5] = { 0x00, 0x04, 0x02, 0x26, 0x07 };
uint8_t m_rxreqa_buf[11] = { 0x00 };
/* Anti-collision */
uint8_t m_txantcl_buf[6] = { 0x00, 0x04, 0x03, 0x93, 0x20, 0x08 };
uint8_t m_rxantcl_buf[10] = { 0x00 };
/* rfid_send_reqa()
*/
void rfid_send_reqa()
{
send_cmd(m_txreqa_buf, sizeof(m_txreqa_buf), m_rxreqa_buf, sizeof(m_rxreqa_buf), 1);
}
/* rfid_send_anticl()
* Send anti-collision sequence to tag
*/
void rfid_send_anticl()
{
send_cmd(m_txantcl_buf, sizeof(m_txantcl_buf), m_rxantcl_buf, sizeof(m_rxantcl_buf), 5);
}
/* send_cmd()
* Send SPI command in 'tx' of length 'tx_len' and pass a 'rx' buffer of 'rx_len'
* for the device to write its response to.
* Wait for 'delay_ms' milliseconds after finishing this transaction, if required.
*/
void send_cmd(uint8_t *tx, size_t tx_len, uint8_t *rx, size_t rx_len, int delay_ms)
{
nrf_drv_gpiote_out_clear(RFID_CS_PIN);
spi_xfer_done = false;
APP_ERROR_CHECK(nrf_drv_spi_transfer(&spi, tx, tx_len, rx, rx_len));
/* Do not wait for transfer done, as we are in a timer that will pick up the event to handle the return from spi */
nrf_delay_ms(delay_ms);
}I then wait on an interrupt from the rfid device to tell me its ready to have data read, at which time I do an spi transfer with a read command.
The REQA comes back as follows (I have verified this is correct)
<info> app: SEND_REQA
<info> app: Pin change detected!
<info> app: Transfer completed
<info> app: Received:
<info> app: 0D 80 05 04 00 28 00 00|.....(..
<info> app: 00 00 00 |...
<info> app: RECV_REQA
```
whereas the anti-collision just does this:
```
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
... (elided, same as above)
<info> app: SEND_ANTI_CL
<info> app: SEND_ANTI_CL
<info> app: Pin change detected!
<info> app: Transfer completed
<info> app: Received:
<info> app: 0E 81 00 00 00 00 00 00|........
<info> app: 00 00 |..
<info> app: RECV_ANTI_CL
Eventually just erroring out with a seemingly undefined error.
Per what I can tell I am sending the correct Anti-Collision request for the protocol I am using. I am reading a MIFARE Classic 1K ISO 14443-3A.
I'm not seeing why the device doesn't respond to the anti-collision request.
If anyone has any ideas, I would be grateful?
2019-07-04 9:29 AM
Hi,
see https://community.st.com/s/question/0D50X0000B0xPsbSQE/cr95hf-error-code-0x81 for a similar issue.
0x81 means invalid command code but in the present case this probably means that some data are corrupted on the SPI link.
A SPI trace would be needed to do a timing analysis.
Rgds
BT
ST25 NFC / RFID Readers – Xx95HF Series
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.