2015-01-14 6:30 PM
Hi all,
I have a project in which I have to use MICS band for data telemetry in an implantable device. Can I use the SPIRIT1 for MICS band which centers at 403MHz? (I think the TI CC1101 can be configured to do it, so should be the same for the SPIRIT1).If it is possible, then I guess I can still use the reference BOM for 433MHz for my design and the only thing I need to change is to configure the frequency base and center frequency to 403MHz through the Spirit1DK GUI?I'm looking forward to hearing from you all,ThanksQuyen2015-01-15 2:06 AM
Hello,
yes, you can use the SPIRIT1 in the aforementioned MICS band. Just set the center frequency to 403MHz through the GUI and you're done!Regards,GaetanoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.