Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF01SA firmware update

Posted on December 26, 2014 at 17:50After firmware update, module does not working.I was using a cople firmware versions:-- SPWF01S-140512-703c969-RELEASE-main.bin-- SPWF01S-140805-3f58d6b-RELEASE-main.bineach one is does not working.As start addres...

How to read ADV data

Posted on February 02, 2015 at 15:43I'm trying to read ADV data sent from a sensor device to my BLUENRG device.I can see the ADV data with a sniffer, but I can't have my device to pass it up to my app.What HCI command should I send to the BLUENRG de...

philippe1 by Associate II
  • 2045 Views
  • 5 replies
  • 0 kudos

BlueNRG discovery (scan interval) issue

Posted on February 18, 2015 at 12:32Hello, I have some troubles while discovering ble devices: no matter what I set the interval scanning (to aci_gap_start_general_discovery_proc function) procedure lasts 10 seconds. Can I somehow reduce the duratio...

Run into some troubles using the reader CR95HF

Posted on February 17, 2015 at 11:24Dear All, We designed a RFID reader using the chip CR95HF. We use quite old SRI4K tags. We used the ST lib (lib_SRIX4k.c from the MMY Application Team) that manages this tag. The hardware design follows the typica...

tlamotte9 by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos

bluenrg 6.4 update - which file to use

Posted on January 08, 2015 at 23:25Hi, I have a STEVAL-IDB002V1.Which image file to use to update the BlueNRG stack to 6.4. bluenrg_6_4_Mode_2-16MHz-XO32K. img orbluenrg_6_4_Mode_2-16MHz-XO32K_HCI.imgWhat is the difference between them?Thanks

dimitar by Associate II
  • 1479 Views
  • 2 replies
  • 0 kudos

BlueNRG JTAG pins

Posted on January 13, 2015 at 23:07On STEVAL-IDB002V1 daughterboard there are JTAG pins connected to BlueNRG(pins 8-11). Is they have any use for user application? #bluenrg

confucij by Associate II
  • 1015 Views
  • 1 replies
  • 0 kudos

SPWF01 limitations

Posted on January 13, 2015 at 16:29Hi,    we are designing a VoIP (SIP/RTP) device with a stm32 microcontroller. It must also have WiFi connectivity, so SPWF01 would be a natural choice. However we've run into limitations of built-in TCP/IP stack wh...

etesial by Associate
  • 1502 Views
  • 2 replies
  • 0 kudos

Can I use of SPIRIT1 for MICS band(403MHz)?

Posted on January 15, 2015 at 03:30Hi all,I have a project in which I have to use MICS band for data telemetry in an implantable device. Can I use the SPIRIT1 for MICS band which centers at 403MHz? (I think the TI CC1101 can be configured to do it, ...

quyen by Associate
  • 1098 Views
  • 1 replies
  • 0 kudos

Spirit1 Evaluation

Posted on December 19, 2014 at 21:13From the landing page on the SPIRIT1 Radio, if i want to operate 915/922 MHz Band - what is required to get started?  Can I use two of the Dongles evaluation modules - STEVAL0IKRV001V5 (on a computer perhaps with ...

rick2399 by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.