2017-11-03 2:42 AM
Hello to everyone.
I have a project I use blueNRG-1
I have problems with energy consumption in the project
no problem in advertising mode and connection status
current in connection status : ~ 250uA
current in advertising mode : ~50uA
But;
current in discovery mode : ~4mA
battery voltage drops to 2.4v at 4mA current
I use CR2032 3V battery.
is this a special case for discovey mode or am I doing something wrong?
my summary code;
uint8_t Start_Discovery_Proc(void) // start discovery procedure
{
uint8_t ret;
ret = aci_gap_start_general_discovery_proc(DISCOVERY_PROC_SCAN_INT, DISCOVERY_PROC_SCAN_WIN, PUBLIC_ADDR, 0x00);
BlueNRG_Sleep(SLEEPMODE_NOTIMER,0,0);
if(ret != BLE_STATUS_SUCCESS)
{
return 0x00;
}
return 0x01;
}
uint8_t Stop_Discovery_Proc(void) // stop discovery procedure
{
uint8_t ret;
ret = aci_gap_terminate_gap_proc(0x02); // GENERAL_DISCOVERY_PROCEDURE
if (ret != BLE_STATUS_SUCCESS)
{
return 0x00;
}
return 0x01;
}
void APP_Tick(void)
{
....
...
.....
if(........)
{
Start_Discovery_Proc();
}
else if(.......)
{
Stop_Discovery_Proc();
}
...
.....
....
}
main()
{
...
...
...
while(1)
{
NVIC_DisableIRQ(UART_IRQn);
BTLE_StackTick();
NVIC_EnableIRQ(UART_IRQn);
APP_Tick();
BlueNRG_Sleep(SLEEPMODE_NOTIMER,0,0);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
is this normal?
Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.