Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

xray format issue

STD120N4F6 dc 20+ , found that the xray format is difference from DC 21+, did there a new PCN during 20+ i'm not sure if these goods are origin. could you pls help to check the labels for me?​

0693W00000WLcjtQAD.png 0693W00000WLclUQAT.jpg 0693W00000WLcl5QAD.jpg 0693W00000WLckIQAT.jpg
demi by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

Interfacing with the X-NUCLEO-BNRG2A1 (BlueNRG-2)

Hi,I picked up a X-NUCLEO-BNRG2A1 (Extension board Lot:2040 for the Nucleo-64 boards), and I am trying to communicate with it through a Nucleo-F411RE Board. I basically generated a project template through CubeMX for the STM32F411RE and included the ...

0693W000008wLRGQA2.png 0693W000008wLRQQA2.png
RrW1 by Associate III
  • 5262 Views
  • 9 replies
  • 0 kudos

BlueNRG-2 DMT firmware question

Hello. I have flashed DTM_UART firmware to my BlueNRG device. I have connected RX/TX pins to IO8/IO11 of the BlueRNG but when I start the device, on serial monitor I only see: and cannot open the device via BlueNRG-GUI.I have picked up the binary fil...

0693W00000WLVYnQAP.png 0693W00000WLWXCQA5.png
LPetr.1 by Senior II
  • 925 Views
  • 0 replies
  • 0 kudos

Wise Studio building firmware for BlueNRG-2

I would like to experiment with BlueNRG FW. I have downloaded BlueNRG SDK from:https://www.st.com/en/embedded-software/stsw-bluenrg1-dk.htmlAnd also I have recently downloaded Wise Studio that I would like to use for building BlueNRG code.In the Wise...

0693W00000WLPSUQA5.png 0693W00000WLPU6QAP.png
LPetr.1 by Senior II
  • 2102 Views
  • 2 replies
  • 0 kudos

where can I get usbpd_core.c document?

hello ,I try to use USB1602 chip build an PD Triger based STM32F103ZE , I download STSW-STUSB010-V1.0.1 and build all the target using MB1303_SINK_ONLY project. I cannot find USBPD_PE_Init(.....) function and some other function defin...

jshen.1 by Associate
  • 1075 Views
  • 1 replies
  • 0 kudos

Configuration of Public Device Address

Dear all,I am currently evaluation the BlueNRG-LP for a new project. I am using the STEVAL-IDB011V1 board and BLE stack v3.1. I've started with the BLESensorDemo to implement our own service. My question is regarding the BLE address.This is how it is...

OKloe.1 by Associate II
  • 4207 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.