Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Simulator is not able to compile even after regenerating from the cubemx interface and then generating with the touchgfx designer.

       Compiling simulator/main.cpp       Linking build/bin/simulator.exe       ../Middlewares/ST/touchgfx/lib/win/mingw32/libtouchgfx.a(PainterRGB565Bitmap.o):(.text+0x307): undefined reference to `touchgfx::paint::rgb565::lineFromRGB565(unsigned sh...

rohan_m by Senior
  • 2144 Views
  • 3 replies
  • 0 kudos

ST4SIM-200M not conecting to network

Hi,I have a custom hardware SIM800F with standard Vodafone IT SIM card and it has always worked great.We are now upgrading the hardware to eSIM (and in the future to SIM7000E), I can read the ICCID and activated the eSIM on TruPhone.com but when it t...

FBert.6 by Associate II
  • 1055 Views
  • 0 replies
  • 0 kudos

AT_RX_TIMEOUT from downlink request using AT modem commands (ST The B-L072Z-LRWAN1 LoRa®/Sigfox™ Discovery kit )

I am using the CMWX1ZZABZ in the ST The B-L072Z-LRWAN1 LoRa®/Sigfox™ Discovery kit with STM32CubeExpansion_SFOX_V1.1.0. The application being used is the Sgfx_ModemAT. I have successfully sent data to our Sigfox backend, I also see from the backend t...

PJows by Associate
  • 1116 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.