2021-08-23 12:21 AM
2021-08-23 2:31 AM
Hi,
SMPS voltage is settable as in page 74 of the datasheet PM_CONF0, you should configure SMPS_LVL_MODE in PM_CONF1 too :
void EnableBoostMode( void )
{
uint8_t tmp;
S2LPSpiReadRegisters(PM_CONF1_ADDR, 1, &tmp);
tmp &= (~SMPS_LVL_MODE_REGMASK);
tmp |= SMPS_LVL_MODE_REGMASK; /*< SMPS_LVL_MODE for Rx and Tx or just Tx >*/
*(uint8_t*)&g_xStatus = S2LPSpiWriteRegisters(PM_CONF1_ADDR, 1, &tmp);
S2LPSpiReadRegisters(PM_CONF0_ADDR, 1, &tmp);
tmp &= (~SET_SMPS_LVL_REGMASK);
tmp |= SET_SMPS_LVL_1_8V; /*< Maximum value >*/
*(uint8_t*)&g_xStatus = S2LPSpiWriteRegisters(PM_CONF0_ADDR, 1, &tmp);
}Andy.
2023-01-25 11:36 PM
Hi,
in my FK433V2 evaluation board I can't reach 16 dBm.
I set:
I this condition I measure 12,9 dBm in CW with the spectrum analyzer.
If I set SMPS_LVL to 1500 mV the measured power is 11,6 dBm.
Is there a limitation of the FK433V2 evaluation board?
Thank You
Massimiliano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.