Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN Transmit Loopback Mode

Hello all,I would like to put the CAN2 interface into operation on a NUCLEO STM32F466RE board. For this purpose I have programmed an example in which a BYTE array HELLO is to be sent in the loopback.If I now pass the TxHeader Struct to the HAL_CAN_Ad...

0693W00000Y9cC4QAJ.png
MZimm.3 by Associate II
  • 6184 Views
  • 10 replies
  • 1 kudos

Resolved! STUSB4710: Default Configuration Confirmation

Hello,I apologize if the answer is obvious but I want to confirm my understanding for the STUSB4710 (USB-C PD controller). Section 4.1 of the datasheet mentions that the default values for the voltage and current settings, which require NO I2C progra...

0693W00000Y9dfbQAB.png
KMew by Senior III
  • 2800 Views
  • 3 replies
  • 0 kudos

The right MCU for ILI9341 driver.

Hello everyone,Please I'm designing a new product and I choosed to use the driver ILI9341 for a 2.8" screen.Now I would like to know if there are some minimal performance of the MCU because I wanted to use the STM32F030C6T6TR. Will it work correctly ...

lonkenzo by Associate II
  • 5882 Views
  • 7 replies
  • 0 kudos

BlueNRG-2

Hi, I have a STEVAL-ID008V2 evaluation board which has a BueNRG2 BLE chip. SDK that I got from the ST website has project examples for this evaluation board. Looking at the codes examples, below method handles the low power mode functionality.  /* D...

RAlma.1 by Associate III
  • 3716 Views
  • 4 replies
  • 0 kudos

How should I receive with S2LP?

Hello, I am trying to receive data in an S2LP, I am successfully sending data using TX FIFO and normal mode, now I want to receive it.However I can't seem to make it work, I'm just reading from SPI to 0xFF

GM.4 by Associate
  • 1557 Views
  • 1 replies
  • 0 kudos

RHFLVDS2281 ibis model problem

Hi,I'm simulating the behaviour of the RHFLVDS2281. When I use this buffer to drive LVDS nets connected connected to RFHLVDS32 diff input, the LVDS signals have really bad behaviuor.I've tried to substitute the driver RHFLVDS2281 with the RHFLVDS31 a...

DSass.2 by Associate
  • 939 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.