Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Alternative of X-CUBE-BLE2 for BLUENRG-LP series

Hi, CubeMX offers two software packs for BLE boards using BlueNRG chips as Bluetooth modules/slaves, one pack for BlueNRG-M and one for BlueNRG-2.However, I could not find one pack for BlueNRF-LP. There is, however, a module called X-CUBE-BLEMGR, but...

Yaxit by Associate II
  • 1457 Views
  • 1 replies
  • 0 kudos

RE-programming SPBTLE-1S from beacon mode to BLE

I bought from gilisymo a ToF sensor with integrated BLE based on SPBTLE-1S from ST. Right now the BLE is setted in beacon mode to save energy but i would like to pass to std BLE communication in a way to acquire the signal at fixed frequency. Unfortu...

rdi c.1 by Associate
  • 1135 Views
  • 1 replies
  • 0 kudos

RSSI value not changing in BLE Mesh Network?

Hello ST,@EMECH​ ​I am using BLE_MeshLightingProvisiner sample project. We try to trace the RSSI value from the below mentioned function:: BLEMesh_NeighborRefreshedCallback(const MOBLEUINT8* bdAddr,                     MOBLEBOOL provisioned,         ...

How to emulate BlueNRG-2n with BlueNRG-2

Hi,We have a custom board with BlueNRG-2 and wants it to act as a co-processor so it can be controlled through SPI from another MCU (STM32L4R9).The BlueNRG-2 has been flashed with STSW-BNRG2N-V320 firmware through the bootloader interface.DIO0 SCKDIO...

CBras by Associate II
  • 1202 Views
  • 0 replies
  • 0 kudos

What is the maximum SPI speed and MCU system clock which can be configured for using BlueNRG2-M2SP module with it

Hello, in the X-CUBE-BLE package this document STMicroelectronics.X-CUBE-BLE2_GettingStarted.pdf says the maximum SPI frequency could be 1Mbits/s . In high perf MCU running at SysClock >500 Mhz , is it possibe to interface BlueNRG2 with it?using Cl...

darla14 by Senior
  • 9525 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.