cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile BLE GATT Characteristic Editing

byrnep8
Associate

Hi,

When editing the GATT characteristic in the provided software for the SensorTile, I cannot increase the size of the payload being transmitted. Even after altering the charValueLen variable, this doesn't appear to affect the length of the packet being sent (In screenshots below edited to be increased to 40 Bytes instead of 8 Bytes):

byrnep8_3-1689201716475.png

 

byrnep8_1-1689201528729.png

byrnep8_2-1689201574962.png

If there is another variable I'm missing to increase the packet length could somebody help me out?

Thanks

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.