Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG UART bootloader: 'go' command question

Hi,Based on AN4872, I managed to get the id, version, erase, read and write memory commands working. I'm able to erase the entire flash of a BRNG-M2SA or BNRG-M2SP and write a pre-built example bin file to the flash and read it back, without errors.H...

Wingunder by Associate III
  • 1930 Views
  • 2 replies
  • 0 kudos

Regarding the thermal data for the parts.

Hi team, Kindly assist us the below mentioned queries.For the some ST microelectronics part data sheet, can not specify the thermal parameter such as junction to case thermal resistance and junction to board thermal resistance. we need those values f...

L9663

Direct interface of communication interface Is the transceiver directly connected to the PSI5 interface of the ECU

JL1 by Associate II
  • 1210 Views
  • 1 replies
  • 0 kudos

BlueNRG-LP beacon example not discoverable

Ive been trying out the different examples on the navigator, and have noticed when using my ble scanner, my device cannot discover the beacon example. I have compared the code with the sensor example which is discoverable and they are very similar ap...

100Vref by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

BLE Whitelisting

My BLE (BlueNRG-MS) application has to offer the following functions and I'm not sure what's the correct approachI need to have a pairing mode where a central device can connect. I think this is achieved by using aci_gap_set_discoverable() with NO_WH...

aj.sk by Associate III
  • 6870 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.