Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not able to send data from BlueNRG LPS

Hi Everyone,I'm using BlueNRG LPS as a network co-processor with STM32L4 Nucleo Board. I'm sending 30 bytes data in every 10ms from stm32 to bluenrg LPS in Non-Block manner, and after 3000 bytes I have to send to packet end command (blocked). So ther...

rshar.21 by Associate II
  • 896 Views
  • 0 replies
  • 0 kudos

TX problem with S2-LP

Hello.I have a problem with S2-LP. I can’t switch S2-LP on a custom board to the TX state. I get the error 0x14 "Error state due to a failure in LOCK operation". The same firmware with the module RC-S2LP-868 works without errors. As an example for th...

ST2378E is not working properly. TT

Hi. I have two level shifters, ST2378e and ADG3308.But, all of them are not working propoerly. Oscilloscope displayed following video.https://youtu.be/JwTMTi1wS8w I had connected pins properly and checked many times.VL(3.3v), VCC(5.0v) and GND OE pin...

Sellyette by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

EVKITST87M01-1 development kit

Hi,There is an introduction on the EVKITST87M01 development kit in the flyer found here: fl2311st87m01.pdf, however, I could not find anywhere online to purchase it. Just wondering if it is available yet?Thanks,Olive

Olive by Associate III
  • 1221 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.