2015-10-06 7:31 AM
2015-10-07 12:53 AM
Hi Mark,
var config is enough to enable flow control. save and reboot.This is how module's RTS/CTS lines works:- CTS stops module's UART TX line. Used when external host is not ready to accept data on its own UART RX line;- RTS signals to external host that it must stop sending datas to module. When DataMode is enabled, and a continuous stream is incoming, RTS switchs state when internal buffers are full (NOT after every byte, as default behaviour on some MCUs), and socket server must output that bytes over the air to empty buffers. When in CommandMode, RTS should never switch since buffer are bigger than ATcmd length (be sure to always expect/wait OK/ERROR).If you think flow control is not working, I suggest an higher baudrate (921600), and an oscilloscope on RTS line.What's your use case? Socket server, payload size, sending rate, etc?Ciaoj2015-10-07 1:21 AM
2015-10-07 1:53 AM
2015-10-07 3:06 AM
Jerry,
Using: # console1_speed = 921600 # console1_hwfc = 1 What I am seeing is this: I am writing data to the module (in data mode) as a series of chunks. Each chunk consists of a 4 byte header and up to 1024 bytes of data. If I write the chunks with no delay between them, I get corruption. If I insert a 50 mS delay between each chunk (still using the same baud rate), then everything works OK but, of course, the throughput is poor. At no time does the module's RTS line change state. Cheers, Mark2015-10-07 4:19 AM
Mark,
did you already take a look at hands-on pdf? Just to be sure that we are aligned.There are some constraints in using socket server: buffer size, timeouts, and so on.There is also a config variable to reduce default timeout value (250ms, huge, to allow customers to play with the module and hyperterminal).Let me know if hands-on is not covering your current experience.Ciaoj2015-10-07 4:29 AM
2015-10-07 4:53 AM
In attach hands-on for FW3.4.
Let me explain ip_sockd_timeout variable, and socket server too. There are some tips to help socket usage.•
Concerning Buffer usage, it is sent out when
•
Timeout expires (none byte is received over UART for ''ip_sockd_timeout''milliseconds)
•
Buffer is full (Note that buffer is 1Kb in size)
•
Concerning timings:
•
Every byte is placed in the Buffer while no Timeout is found. When Timeout occurs, Buffer is sent to Client
•
Every Escape Sequence
must
be followed by a Timeout. If Escape is followed by further bytes, the whole “
Escape+bytes
�? sequence is sent to Client;
In order to free the buffer for next operation, a Timeout should go before every Escape Sequence. In this case, bytes before Escape Sequence are sent, the buffer is freed, and so the Escape Sequence is correctly received and understood. Otherwise, if the Escape Sequence is sent at the end of buffer, around 1Kb size limit threshold, the whole “
bytes+Escape
�? sequence is sent to client in 2 different packets.
Hope it helps j ________________ Attachments : wifi_Training_-_Hands_On_-_FW3.4.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I12v&d=%2Fa%2F0X0000000bmw%2FvQOrvIv_nJ33p_vKM9q87yGHhBVn4lHxTr79hl_nhIw&asPdf=false2015-10-07 5:51 AM
Gerry,
Thanks for the updated hands on. I have reduced ip_sockd_timeout down to 10mS and my comms protocol is much snappier! However, I am still not seeing any RTS activity by the module and wonder if I am not actually filling the module's buffer space enough to trigger the flow control. How much data can be sent to the UART before the buffer fills and RTS goes high? Is the flow control definitely enabled in data mode? I have no way of telling. It remains a mystery why my data stream is getting corrupted but, right now, it's not critical to use the higher baud rate so I can fall back to using a lower baud rate or use the 50 mS delay between chunks if a solution isn't found. Cheers, Mark2015-10-07 10:38 AM
How much data can be sent to the UART before the buffer fills and RTS goes high?
Since there is more than one buffer, and since buffers emptying depends also on protocol used (TCP/UDP) and network traffic, I cannot say what's the limit. What I can say for sure, is that RTS works fine, and data loss is avoided using flow control.Is the flow control definitely enabled in data mode?Yes. When config var is set, both CommandMode and DataMode are using flow control. RTS switches if/when needed.It remains a mystery why my data stream is getting corruptedLet me know if you find any module issue!Thanks for all of your feedbacks! They will be used for sure!jWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.