2015-10-11 6:14 AM
Hi everybody,
I have troubles to connect the SPWF01 with an AP using WPA2 privacy mode. When I try to connect, after Wind 25: association successful, I receive Wind 40: deauthentication:1 +WIND:19:WiFi Join:00:04:ED:61:FB:18 +WIND:25:WiFi Association with 'Alison' successful +WIND:40:WiFi Deauthentication:1 +WIND:74:Rejected found Network I have another AP and I can link with it using the same security mode and the same password, hence my code should be right. +WIND:19:WiFi Join:14:CC:20:9C:D5:4D +WIND:25:WiFi Association with 'Alison_EXT' successful +WIND:51:WPA Handshake Complete +WIND:24:WiFi Up:192.168.1.110 I did a scan and the APs are in WPA2 for sure: 1: BSS 00:04:ED:61:FB:18 CHAN: 06 RSSI: -59 SSID: 'Alison' CAPS: 0411 WPA2 2: BSS 14:CC:20:9C:D5:4D CHAN: 06 RSSI: -79 SSID: 'Alison_EXT' CAPS: 0431 WPA WPA2 WPS I think it could be a security issue because I can connect to the bad AP in Open mode. I searched the web for deauthentication:1. It is ''Unspecified failure'', so I can't have any clue from it. The module has the last FW version: 150410-c2e37a3-SPWF01S. Could you give me any hint? Thank you, Paolo2015-10-11 6:30 AM
Ciao Paolo,
can you please share AP model, and FW version too?ciaojerry2015-10-12 1:43 AM
Ciao Jerry,
AP model: Digicom Michelangelo Wave FW version: 2.7.0.23(RUE0.C2)3.5.10.1 Paolo2015-10-12 1:54 AM
Can I ask you to update router FW to the lastest one?
Versioni RUE: 2.11.62.2RE0 - Versioni ZUE: 2.9.5.3ZUEThanksj2015-10-12 3:38 AM
I'm sorry, I don't do it...
my AP works well and I don't want to break its equilibrium. It hasn't given me a problem in years of work. Paolo2015-10-12 12:37 PM
Ciao Paolo,
do you see the issue using all of the following settings (WPA mode/Cipher Suite)? - WPA/TKIP - WPA/AES - WPA2/TKIP - WPA2/AES Thanks Ciao Salvatore2015-10-13 1:28 AM
Ciao Salvatore, Gerardo,
I upgraded the AP FW and the problem is desapeared! I have another oddity for you. Trying to connect to the AP in all the privacy modes I noticed that using WEP the SPWF01 gives me Wifi Up even though the password was wrong. Module however was not reacheble. This still happens after the AP FW upgrade. Paolo2015-10-13 1:34 AM
Ciao Paolo,
in attach an howto use WEP. It's not so easy like WPA Let us know if problem is still there. Thanks jerry ________________ Attachments : WEP_key_config.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Em&d=%2Fa%2F0X0000000bn5%2FiVT6evhEiXIPE64aqAwag28X35.VJZYdvGt5SBZHQiE&asPdf=false2015-10-13 1:43 AM
Hi Gerardo,
I'm not saying that WEP doesn't work.I was able to
use it
. I'm saying that the module says connected even if it isn't. Paolo2015-10-13 1:12 PM
Hi Paolo,
could you please confirm that another device (PC, smartphone) works fine with the AP in WEP mode? I found some threads on public forums where users claim issues after connecting a PC to Michelangelo Wave (in WEP mode). Could you please also share with us the details of the WEP config used (WEP authentication, WEP encryption, Key 1 configured)? Thanks Ciao SalvatoreWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.