Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32cube SPI DMA for MAX31865 chip

Posted on December 11, 2016 at 15:05i have all my initialization code generated for STM32F217 SPI DMA  using STM32CUBE as MASTER. Does anyone have a good c code example of the main() with infinite loop while() code sending and receiving data and the...

Resolved! Static IP Address

Posted on December 14, 2016 at 09:50Hi Everyone !I am using  SPWF01S wifi module.I would like to assign static IP for my module, so that my module will have same IP address even when connected with different networks.I used the following AT Commands...

Nandy K by Associate II
  • 2115 Views
  • 3 replies
  • 0 kudos

SPI and BlueNRG sleep mode

Posted on July 23, 2016 at 04:31After SPI bus activity stops, how long until BlueNRG goes into sleep mode? Document UM1755 BlueNRG Bluetooth®LE stack application command interface (ACI) implies the time is 2 mS.  This is important because there is a...

rdscliff by Associate II
  • 1039 Views
  • 1 replies
  • 0 kudos

Python scripting for BlueNRG

Posted on July 12, 2016 at 20:24Can BlueNRG scripting work as a full Python program?  Questions I have: Can scripts be run in a normal Python debug environment rather than using BlueNRG_Script_Launcher to run?Can I import standard Python modules i...

rdscliff by Associate II
  • 2593 Views
  • 5 replies
  • 0 kudos

aci_gatt_update_char_value error

Posted on December 08, 2016 at 00:37static const char *name = 'ThisaTest1';aci_gatt_update_char_value(&service_handle, dev_name_char_handle, 0, strlen(name), name) returns 0x47.From the API document 0x47 is 'Error'

recover idw01m1 after wrong reflashing sequence

Posted on December 05, 2016 at 22:13Ok, despite alll the warnings in the instruction sheet.... I wrongly reflashed one IDW01M1 module. Basically I wrote the firmware from the first page, and I suppose this compromised the bootloader.Is there any way...

infor by Associate III
  • 1099 Views
  • 2 replies
  • 0 kudos

Removing the spwf01sx cgi files.

Posted on December 08, 2016 at 09:13Hi, I was wondering that if it is possible to delete the HTML and CGI file system from the module.?P.S: I can see from the documentation that it is possible to disable/enable the feature. My concern is to permanen...

pouya by Associate II
  • 987 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.