Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP strobe COMMAND_RX after DATA discarded EINT

Can someone tell me why the need to put the Receiver back in Receiver mode after getting a DATA_DISCARDED Interrupt, (many examples are using this), I'd like to only get interrupted when the preamble and sync bits match, I find it excessive (every fe...

xarion by Associate II
  • 1202 Views
  • 1 replies
  • 0 kudos

RSSI value of a node without mesh network

hello,I want to know if it is possible to get the RSSI value of a node with this function in BLUENRG-1 without the mesh network.tBleStatus hci_read_rssi (uint16_t Connection_Handle, uint8_t *RSSI);Can I use this if yes how? Because I am getting only ...

FChou by Associate II
  • 1488 Views
  • 2 replies
  • 0 kudos

SPWF01SA Deauthentication FW 3.6

Hi,I have a problem with SPWF01SA WiFi module with FW 3.6. The module is connected to a WiFi network, generated by a router (STAtion Mode), with active DHCP. A socket server is opened on port 80. I have seen that after a day the module IP is changed ...

Is it possible to perform asset tracking/indoor localization or to measure RSSI value on a BlueNRG-1/2 board in a bluetooth mesh network ?

I want to track/locate the position of a bluetooth mesh node. I am currently using three BlueNRG-1 based STEVALIDB007v1 boards and an android smartphone to form a bluetooth mesh network in which smartphone reads sensor data from mesh nodes. I did som...

MH1 by Associate II
  • 3231 Views
  • 8 replies
  • 0 kudos

RSSI value of a mesh network node

helloi would like to know if it is possible to get the RSSI value of a node while it is provisioned in the mesh network. i am testing with 3 steval IDB007V2 evaluation board and i want to know how to get the RSSI value of one node A in mesh network w...

FChou by Associate II
  • 2640 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.