2018-12-10 5:49 AM
Hello,
I am using the BlueNRG LE stack to set my BLueNRG-MS device discoverable to Android app on smartphone/tablet.
I am using the aci_gap_set_discoverable function from LE stack with following parameter:
#ifdef _DEBUG
USART_printf("*** Setting discoverable mode ***");
USART_printf("Adv MIN = %d ms", (CONFIG_global_configuration.min_advertising_interval*625)/1000);
USART_printf("Adv MAX = %d ms", (CONFIG_global_configuration.max_advertising_interval*625)/1000);
USART_printf("Conn MIN = %d ms", (CONFIG_global_configuration.min_connection_interval*1250)/1000);
USART_printf("Conn MAX = %d ms", (CONFIG_global_configuration.max_connection_interval*1250)/1000);
#endif
/* set the device in general discoverable mode */
ret = aci_gap_set_discoverable(
ADV_IND,
CONFIG_global_configuration.min_advertising_interval,
CONFIG_global_configuration.max_advertising_interval,
PUBLIC_ADDR,
NO_WHITE_LIST_USE,
strlen(bluetooth_device_name) + 1,
local_name,
0,
NULL,
CONFIG_global_configuration.min_connection_interval,
CONFIG_global_configuration.max_connection_interval
);where:
Adv MIN = 500 ms
Adv MAX = 1000 ms
Conn MIN = 12 ms
Conn MAX = 25 msI have also instrumented the EVT_LE_CONN_COMPLETE and EVT_LE_CONN_UPDATE_COMPLETE events to get more information at connection establishment:
case EVT_LE_CONN_COMPLETE: /* BlueNRG connection event */
{
/* connection complete event: get the related data */
evt_le_connection_complete *cc = (void *)evt->data;
connection_handle = cc->handle;
#ifdef _DEBUG
USART_printf("*** Connection complete ***");
USART_printf("Connection status = %d", cc->status);
USART_printf("Connection handle = %d", cc->handle);
USART_printf("Connection interval = %d", cc->interval);
USART_printf("Connection latency = %d", cc->latency);
#endif
}
break;
case EVT_LE_CONN_UPDATE_COMPLETE: /* BlueNRG connection update event */
{
/* connection complete event: get the related data */
evt_le_connection_update_complete *cuc = (void *)evt->data;
connection_handle = cuc->handle;
#ifdef _DEBUG
USART_printf("*** Connection update complete ***");
USART_printf("Connection status = %d", cuc->status);
USART_printf("Connection handle = %d", cuc->handle);
USART_printf("Connection interval = %d", cuc->interval);
USART_printf("Connection latency = %d", cuc->latency);
#endif
}
break;Then while connecting to device with application, I get the following log:
14:28:00: *** Connection complete ***
Connection status = 0
Connection handle = 2049
Connection interval = 39
Connection latency = 0
*** Connection update complete ***
Connection status = 0
Connection handle = 2049
Connection interval = 6
Connection latency = 0
14:28:01: *** Connection update complete ***
Connection status = 0
Connection handle = 2049
Connection interval = 39
Connection latency = 0I am not trying to update the connection at startup, so can you indicate me if there is a reason 3 events are logged, with the connection interval parameters out of specified MIN/MAX range ??
Thank you in advance,
Regards
R
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.