Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST8500 FSK modulation

Hi, I am evaluating to use the ST8500 module as alternative part of the ST7538Q.In our application we have a custom protocol over power line with FSK modulation.Looking all the documentation related to ST8500 I found that it is possible to configure ...

Resolved! BlueNRG-LP maximum advertisement delay.

Hello,When I try to set advertisement delay more than 10000ms, the function aci_gap_set_advertising_configuration return an error 0x82 (BLE_STATUS_INVALID_PARAMS). According to the function declaration, it must be ok:/* .... * @param Primary_Advertis...

jbie by Associate II
  • 4212 Views
  • 7 replies
  • 0 kudos

SPIRIT1 VCO autocalibrate errata

Posted on August 14, 2015 at 19:20So if I want to hop to various frequencies I need to calibrate the VCO each time. That's fine and expected. The SPIRIT1 has a fantastic auto calibration time of only around 50us - one of the features that make it at...

kzkaram by Associate II
  • 2292 Views
  • 3 replies
  • 0 kudos

3-port switch KSZ8863RLL + STM32

Hello! The task is to implement a device with two-port Ethernet. To do this, I developed a circuit, connected the STM32F207 controller to the KSZ8863RLLI Ethernet transceiver via RMII. The controller and the transceiver are connected according to the...

BNiki.1 by Associate
  • 1793 Views
  • 1 replies
  • 0 kudos

Resolved! Connect to TLV493D-A1B6 over I2C

Hi folksI am currently trying to communicate with the TLV493D-A1B6 3D hall sensor. As board, I'm using the NUCLEO-F103RB. To make sure I didn't mess up any connections or anything else, I verified my setup with an ADS1015 adc which I can read out ove...

Jiimmy by Associate II
  • 5105 Views
  • 5 replies
  • 0 kudos

STM32, SPI communication and SX1280.

Dear everyone,I'm trying to use a SX1280 for RF connectivity.My dev board is the official... the SEMTECH "SX1280ED1ZHP", it's included a nucleo + daughter board with SX1280.My diffculty is that a not able to read correctly a register with a know valu...

Capture d’écran 2024-11-28 143754.png Capture d’écran 2024-11-28 143319.png TEK0001.JPG TEK0002.JPG
JL_Loyd by Associate II
  • 1913 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.