Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! S2-LP with Balun and RF Front-End

Hello,I am currently reviewing the S2-LP transceiver for high-bitrate/long-range communication in the 915MHz band. To achieve that, I want to interface an S2-LP with a Skyworks SE2435L front-end, as shown in the FK915V1 Evaluation board. I would like...

Chalumo by Associate
  • 3852 Views
  • 3 replies
  • 1 kudos

S2-LP custom parameters

Hello, I'm evaluating the use of the evaluation kit and the evaluation software for the S2-LP to generate the OOK signal, In the software I can't modify the Preamble to a custom pattern, another thing is to be able to place the ID address (I can not ...

User2501_0-1730819906936.png User2501_0-1730804919129.png
User2501 by Associate II
  • 1454 Views
  • 1 replies
  • 0 kudos

BlueNRG-MS data throughput

Hi, I'm fighting with a low data throughput of the BlueNRG-MS. The BlueNRG based device acts as a peripherial and sends notifications periodicaly to PC or Android app. The problem is I'm not able to achieve a higher data rate than approx. 1 kB per se...

ZSara by Associate
  • 1688 Views
  • 2 replies
  • 0 kudos

LVDS transmitter output resistor

Hello,I'm working on a schematic where an LVDS transmitter (DS90C385AMT_NOPB) connects to a display through a connector. In my design, a 100-ohm termination resistor is placed between the differential pairs TXOUT and RXIN, as shown in the second imag...

Figure 1.png Figure 2.png Figure 3.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.