2019-01-16 12:11 PM
Hi,
I'd be grateful for any suggestion what BT module supporting HID I should use to connect BT HID keyboard to the STM32. I see that many popular HC-XX modules support only SPP profile.
There are some modules supporting HID profile but all the examples I found focus only on using them to implement the HID device (not to terminate the connection from the device).
What I want to achieve:
BT_HID_KB-------------------------------BT_HID_Host_Module------STM32
So the BT_HID_Module I am looking for is supposed to have BT Host functionality.
Thanks,
Bogdan
Solved! Go to Solution.
2019-01-17 12:10 AM
One solution I found (not very easy to implement):
RN42 module, HCI mode (the HW offload for profiles is disabled and the whole processing is moved to the host MCU)
https://cdn.sparkfun.com/datasheets/Wireless/Bluetooth/bluetooth_cr_UG-v1.0r.pdf
"In HCI mode, the on-board stack is bypassed a nd the module is put in a state that runs the Bluetooth baseband. The HCI provides a command reference interface to the base-band controller and the link manager, and provides access to the hardware status and control registers. This interface provides a uniform method for accessing the Bluetooth baseband capabilities.
"
2019-01-16 5:22 PM
The suitable forum for this question is: Interface and connectivity ICs
https://community.st.com/s/topic/0TO0X000000BSqXWAW/interface-and-connectivity-ics
-- pa
2019-01-17 12:10 AM
One solution I found (not very easy to implement):
RN42 module, HCI mode (the HW offload for profiles is disabled and the whole processing is moved to the host MCU)
https://cdn.sparkfun.com/datasheets/Wireless/Bluetooth/bluetooth_cr_UG-v1.0r.pdf
"In HCI mode, the on-board stack is bypassed a nd the module is put in a state that runs the Bluetooth baseband. The HCI provides a command reference interface to the base-band controller and the link manager, and provides access to the hardware status and control registers. This interface provides a uniform method for accessing the Bluetooth baseband capabilities.
"
2019-01-17 8:17 AM
After some research:
I will consider the USB Host HID to support BT HID devices (to re-use US Host library for HID devices)
The idea is shown here:
https://blog.tkjelectronics.dk/2013/12/bluetooth-hid-devices-now-supported-by-the-usb-host-library/
There is a small version of USB Host:
http://shop.tkjelectronics.dk/product_info.php?products_id=45
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.