2018-09-30 10:32 PM
S2-LP transceiver, STEVAL-FKI868V1:
it has a feature 'Automatic acknowledgement, retransmission, and timeout protocol engine".
1. Does the acknowledgement automatically come from receiver?
2. Does this feature automatic for S2-LP transceiver or it may be enabled/disabled programmatically?
3. If I want to use a few receivers, is it possible to disable this feature or enable it only for one receiver, which is placed on the longest distance?
Solved! Go to Solution.
2019-01-13 9:24 PM
Hi N.Vadim,
in SDK_StackLlp_B.c it enables the auto ack by default (line 379): S2LPPktStackAutoAck(S_ENABLE);
Please modify according your needs.
Best Regards,
Winfred
2018-12-20 11:33 PM
It depends on your mode, if you are using STack it does an automatic acknowledgement. If you don't want an ACK then use a basic configuration similar to the GUI.
2019-01-13 9:24 PM
Hi N.Vadim,
in SDK_StackLlp_B.c it enables the auto ack by default (line 379): S2LPPktStackAutoAck(S_ENABLE);
Please modify according your needs.
Best Regards,
Winfred
2019-01-18 10:44 AM
Hi Winfred,
thank You very much,
it's rare to see such answers - all according to the questions and nothing redundant.
And it was very usefull for me to get the names of libraries and examples and ever line number in c-file !
Best regards,
Vadim
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.