2019-03-28 10:47 AM
Hi to all.
I'm working on telemetry board:
On SPSGRFC datasheet it's reported up to 500 kbit/s on-air bitrate, sensitivity -118dB and maximum output power 11.6dB, so it should be okay for my purposes (at least up to 3km).
I don't understand if sensitivity is related to a specific bitrate, or is it related to the maximum bitrate avaliable...
Thanks.
2019-03-31 7:16 PM
Hi mbertoni,
The sensitivity will be different with different radio settings including data rate.
Please refer to S2-LP datasheet for more details about sensitivity for different data rates.
DS11896, table 23
https://www.st.com/resource/en/datasheet/s2-lp.pdf
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.