2019-03-21 3:06 PM
Hello,
Is s2-lp RF module supports mesh? If yes, where can'i found mesh stack and how it can be used?
Is below application note describe how can'i configure s2-lp module to work on mesh network? https://my.st.com/resource/en/design_tip/dm00567382.pdf
Thanks in advance.
2019-03-24 6:45 PM
Hi Nasramine,
Please take a look at X-Cube-Sub1,
which includes diddleware library with Contiki OS and Contiki 6LoWPAN protocol stack
with ability of mesh networking.
Thank you.
Best Regards,
Winfred
2019-03-25 1:23 PM
Thanks a lot for your Answer.
In X-Cube-Sub1 i didn't found a complete example with mesh networking. Examples under "X-CUBE-SUBG1\en.x-cube-subg1_firmware\STM32CubeExpansion_SUBG1_V3.1.0\Projects\Multi\Applications\Contiki" didn't describe how to create mesh network
I saw that we have mesh api such as mesh_open, mesh_send..., should these APIs be called just after Stack_6LoWPAN_Init in each node?
Thanks a lot in advance.
2019-03-25 8:52 PM
Hi Nasramine,
For Contiki's mesh samples, please refer to Contiki's document
http://contiki.sourceforge.net/docs/2.6/a00011.html
Best Regards,
Winfred
2019-03-25 11:22 PM
Hi Winfred,
Thanks for Contiki's mesh samples.
All mesh APIs (mesh_open, mesh_send...) should be called after calling API Stack_6LoWPAN_Init (otherwise S2_LP transceiver will not be started and mesh cannot be established)?
Mesh code deployed in each node will be something like this:
int main()
{
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
HAL_EnableDBGStopMode();
MX_GPIO_Init();
USARTConfig();
#if MCU_LOW_POWER
if (USER_CLOCK_FREQUENCY != DEFAULT_CLOCK_FREQUENCY) {
HAL_RCC_DeInit();
LP_sysclk_config(USER_CLOCK_FREQUENCY);
MX_GPIO_Init();
HAL_UART_DeInit(&UartHandle);
USARTConfig();
}
#endif /*MCU_LOW_POWER*/
/* Initialize LEDs */
BSP_LED_Init(LED2);
RadioShieldLedInit(RADIO_SHIELD_LED);
BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
/* Initialize RTC */
RTC_Config();
RTC_TimeStampConfig();
_print_fw_info();
Stack_6LoWPAN_Init();
mesh_open(&mesh, 132, &callbacks);
....
Thanks to correct me if i'm wrong
Best Regard,
Amine
2019-04-05 12:48 PM
Hi Winfred,
Any news please?
Best Regard,
Amine
2019-04-07 6:16 PM
Hi Amine,
You've got the entry.
Please try to replicate Contiki mesh example.
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.