Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enable disable LDC mode

Hi,I really appreciate the reactivity of the forum, thanks a lot.i have some questions:1- When i enable/disable LDC mode using S2LPTimerLdcrMode, and S2LpTimerFastRxTermTimer, i need to run command S2LPCmdStrobeReady and S2LPCmdStrobeRx after each en...

BMoha.19 by Associate II
  • 1304 Views
  • 1 replies
  • 0 kudos

BlueNRG2 - Packet Length extension (Tx direction)

using BlueNRG2, I'm trying to send long packets (> 20 bytes), I added a custom service with characteristic supporting notification and indication with a size = 40 bytes. After the connection established, I send a LL_LENGTH negotiation to update the T...

MBRAI.9 by Associate
  • 895 Views
  • 0 replies
  • 0 kudos

How to rebuilt BlueNRG-2 for UART

I need to update the pins used for UART communication by the BlueNRG-2 chip. I have found documentation that states you can update the source code as necessary. Is there any documentation on how to actually build the target .bin or .hex file after yo...

SBukh.1 by Associate II
  • 3113 Views
  • 4 replies
  • 1 kudos

STEVAL-BLUEMIC-1signal strenght

We are working with 2 STEVAL-BLUEMIC-1 boards, one configured as server and one configured as client. Server is located into a PVC box at about 2/3 meters from the client. We noticed that when we hold in hand the pvc box or when we interpose ourselve...

EBono by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

Resolved! Help Identify this part? 1600N729?

Hi,Can anyone help me identify what ST component this is? It's used in an R/C transmitter I have, it's not old, built in 2019...But I cannot figure out what ST Micro part this relates to?I found the 'STUSB1600', but that doesnt seem to fit with the ...

0693W000000WrySQAS.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.