Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Host interface with BlueNRG-2

I am developing a custom board in which I want to interface a BLE chip and for that, I am looking forward to using BlueNRG-2 in my design. From what I have studied online BlueNRG chips support only SPI based interface with the Host controller. The pr...

user error: reset failed in IAR while and download the debug the lightning_demo project to STEVAL-IDB008V2 in IAR

I'm using the IAR(8.40.1) for flashing the code(Lightning_demo from stsw-bnrg-mesh package) using stlink. After pressing the download and debug icon i'm facing User error: Reset failed.But while flashing with BlueNRG1 ST-Link Utility, I was able to ...

0693W000001cGEiQAM.png 0693W000001cGDVQA2.png 0693W000001cGB6QAM.png
Anitha by Associate III
  • 986 Views
  • 0 replies
  • 0 kudos

Resolved! Only half of the IrDA packages are received correctly

Hi!I have a STM32F765ZITx as master and a STM32F051C8Tx board as slave that im trying to communicated with each other over IrDa. The master is sending 6 bytes (2 startbytes, 1 length of data byte, 1 databyte, 2 checksum bytes) to the slave, which wor...

Hoddy by Associate II
  • 1516 Views
  • 1 replies
  • 0 kudos

M41T83 crystal will not start to vibrate

I use a RTC IC M41T83 in our prototypes and can access this RTC via I2C bus (reading and setting timestamps). Unfortunately the crystal does not start. At startup I set the ST bit to 1 (write address and write a byte via I2C) and then I set the bit t...

TBend.1 by Associate
  • 707 Views
  • 0 replies
  • 0 kudos

Why provisioning did not happen the second time, once unprovisioned the node first-time blemesh mesh app using STEVAL_IDB008V2?

Hi sir/Madam,If we flashed BlueNRG2_Lighting_Demo.bin file using USB micro in STEVAL_IDB008V2 board it was provisioned. If we give commands from models, board doesn't show any change in the led, why? So that we unprovisioned node and tried to provisi...

Anitha by Associate III
  • 924 Views
  • 0 replies
  • 0 kudos

Is BlueNRG-Tile support notifications from more then one characteristics simultaneously, if I considered BlueNRG-Tile as a client??

I am using BlueNRG-Tile chip. I am configuring it as a server. And i am using ST BLE Sensor App as a master. In that i am getting all the services and characteristics displayed on App ,which I have configured at server side. My target is to get notif...

DRamp.1 by Associate
  • 628 Views
  • 0 replies
  • 0 kudos

How can I use the LTDC on a Nucleo and wire it to my Elegoo TFT display shield (which is ILI9341, but only has 8 data pins)?

Sorry if this is a dumb question. I have a Nucleo F767ZI, and I want to wire it to this: http://www.lcdwiki.com/2.8inch_Arduino_Display.There's a tutorial here on how to set up LTDC with an ILI9341 here: http://www.lucadavidian.com/2017/10/02/stm32-u...

NNagy.1 by Senior
  • 1038 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.