Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-2: Dma do not working after wakeup

I;m working on bluenrg-2.The system undergo sleep after 3 minutes if no device connected I have to read the ADC value from DMA.Once the system undergo sleep ,the wake up switch will wake up the board.But after wake up the DMA not working. if(DMA_Get...

RJOY.1 by Associate III
  • 675 Views
  • 0 replies
  • 1 kudos

Need the BOM for BLUENRG-1 schematic.

I am using BLUENRG-1 (QFN package, 32 pin) in my design. I got the schematic of BLUENRG-1 for my design but I am not able to get the value mentioned in the schematic. If anyone has BOM for the schematic please share with me.Please check the attached ...

SShar.11 by Associate
  • 1624 Views
  • 3 replies
  • 0 kudos

Can't find MS5611 device on I2C.

Hello! I recently started working with STM32 microcontrollers and I'm trying to work with a MS5611 sensor with I2C but when I use HAL_I2C_IsDeviceReady function to detect the different devices I have on the I2C it detects nothing. I have check the bo...

Resolved! STPM32 UART protocol details

Hello,I'm working on a driver for a proprietary device that should interface with an STPM32 power meter via UART. I'm at the point of writing some routine to access STPM32 registers without the need of manually compose the UART frames.However, I keep...

DGiov.1 by Associate III
  • 2957 Views
  • 4 replies
  • 0 kudos

STPM34 voltage measuring section - Neutral line directly connect to IC GND Vs Through a series Resistor

Hi All,i am using STPM34 for metering application to measuring the Energy used in the EV charging station.As per the development board design provided by the ST to measure the AC voltage , the Neutral lone is connected directly to the comment GND for...

APK.1 by Associate II
  • 1269 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.