Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About testing mode DTM for SPBT3.0DP2

Hello, We are still using in our design the obsolete SPBT3.0DP2 (we have stock of this part still available), and we need to pass a regulatory test. For this test we need to work in DTM mode (Direct Test Mode). Can anyone tell me if this mode is avai...

BlueNRG2 Standalone Demonstration Application

We have designed a custom board using BlueNRG-2 and are now working on developing applications on the same. However, the Evaluation Tool Software only consist of BlueNRG-1, BlueNRG-2 DK SW package, which we understand is the package for Development k...

KBudk.1 by Associate
  • 947 Views
  • 1 replies
  • 0 kudos

How can I develop firmware for BlueNRG-2 BLE SoC on standalone processor mode (using built in Cortex M0)?

I currently have X-NUCLEO-BNRG2A1 expansion board and have no problem to program it using STM32 Nucleo board in coprocessor mode, but there seems to be no information about "stand alone" programming. What software should I use to develop applications...

Amiel.1 by Associate
  • 2172 Views
  • 4 replies
  • 0 kudos

EVAL-SCS001V1 Sink Voltage setting

Hello,I am playing with the EVAL boardEVAL-SCS001V1, NUCLEO board, and the STSW-STUSB002 GUI software. I am using the PD SOURCE as Globetek Power Module(RR9LZ3000USBCG2(R6B)) , It is generating 20V output voltage at the EVAL board terminal block J10....

NAmam.1 by Associate
  • 1188 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.