Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which one of the "BLE" or "Wi-Fi 802.15.4" is more fit (and suitable) in order to using into the smart wireless network including many sensors.

HelloWe would like to know that, which one of the "BLE" or "Wi-Fi 802.15.4" is more fit (and suitable) in order to using into the smart wireless network including many sensors (when there are more than 4 sensors in the network).Thanks

ST25R3912 calibration

Hi, I'm new with the NFC family. I am have issue with calibration for ST25R3912. I have been read the document but not found any idea. Can anyone give me the suggest to help me calibration for ST25R3912 . Thanks.

TTran.6 by Associate
  • 553 Views
  • 0 replies
  • 0 kudos

BlueNRG 2N - link status function returns 255

I have BlueNrg2N chip in advertising mode and I sometimes have a situation that chip stops advertising on it own and aci_hal_link_status function returns 255 (all status bits are set). Maybe someone have any idea what does it mean and why it happens.

DJędr.1 by Associate
  • 466 Views
  • 0 replies
  • 0 kudos

Is the STUSB4710 VBUS enable mandatory?

HiIs it possible to use the STUSB4710 without the VBUS_EN_SRC switch? In such a way the the VBUS is always sourced from the supply side.I expected this to work, but when I tried it on the STUSB4710A evaluation module, it seems it will not set any PDO...

TNils.1 by Associate II
  • 733 Views
  • 1 replies
  • 0 kudos

STUSB-4710 in STEVAL-ISC004V1 toggling VBus_EN_SRC

Hello,I just got a STEVAL-ISC004V1 kit for evaluating the STUSB-4710 in a USB-PD Application.As described in the manual I connected it to a 24V power supply and connected it to the Nucleo F072RB and the corresponding GUI. I can access the device and ...

LB1 by Associate
  • 842 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.