Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Logs cannot be exported anymore

Started today with my STEVAL-STWINKT1B, with default firmware and an outdated version of ST BLE Sensor app.I was happy, the app connected and I was able to do a first trial, gather some data and export the data as csv by email.After that, I did an up...

SThie.1 by Associate II
  • 1696 Views
  • 2 replies
  • 0 kudos

Why does BlueNRG-1 wake up once 10 seconds?

I used BlueNRG-1 to make 1 minutes wake-up timer. But it seems wake up once 10 seconds. It causes current consumption more about 1.5uA. How to solve it? Detail information is at attach file. My code snipped is as follows. #define SCAN_RESPONSE_TIMER ...

TWu.6 by Associate II
  • 1638 Views
  • 2 replies
  • 0 kudos

BlueNRG-M2 idle power consumption too high

I am building a non-connectable beacon using a BlueNRG-M2SP board, and an STM32L412 MCU as a host, and the power consumption of the M2SP board between advertisment phases is around 24 uA, which is over 10 times higher than what the datasheet says (2....

Enter deep sleep problem of the BlueNrg-2 FreeRTOS

Please let me know below the below status and can't enter deep sleep by Bluenrg-2 FreeRTOS. ​1.vPortSuppressTicksAndSleep( TickType_t xExpectedIdleTime )2. BlueNRG_Sleep(SleepModes sleepMode, uint8_t gpioWakeBitMask, uint8_t gpioWakeLevelMask)3.ble_s...

CKim.18 by Associate II
  • 1820 Views
  • 2 replies
  • 0 kudos

BlueNRG gdbserver for ST-LINK V3

Hello all,I’m just getting started playing around with BlueNRG 1 & 2 devices. I’d like to be able to debug with an ST-LINK V3 not using uVision. I found a patched ST LINK gdbserver in the 3.2.1 DK download but it’s an old version that doesn’t seem ...

svcguy by Associate III
  • 1220 Views
  • 1 replies
  • 0 kudos

S2-LP getting into unknown state (MC_STATE0 is 0x29)

Greetings, I'm configuring the S2-LP to act as a receiver and then strobing the reception. Sometimes the reception works and the S2-LP goes to the RX state as seen from the first 2 bytes of status on MISO . Sometime, randomly, it goes into an unknown...

PNare by Associate III
  • 4348 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.