Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi everyone, does someone know an example of communication of CANOPEN and which evaluation kit iwith STM32 is possible to use it?

For my project, I would like to create a communication (CAN and CANOPEN) with an evaluation kit of ST and an other electronic card and a sniffer to analyse the different weft in the bus. But I'm a novice in this communication so I search an example o...

CMahe.1 by Associate II
  • 679 Views
  • 0 replies
  • 0 kudos

L6362ATR - MTBF/FIT

Hello,can you please provide reliability data (at least a FIT value) for the L6362ATR ?A document would be nice.Best regards,Markus

MNeum.1 by Associate II
  • 846 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-IDP004V1 connection with STM32 Nucleo

Dear Supporters,iam purchanging a STEVAL-BFA001V1B kit and STEVAL-IDP004V1 IO-Link master Board,now i wanted to connect my IO_Link master Board to STM32 Nucleo Board and use Nucleo Board as main Controller. is it possible for data transfer between IO...

GVall.2 by Associate II
  • 2677 Views
  • 4 replies
  • 0 kudos

Wake up b-l072z-lrwan1 from LoRa

Hello,I have 2 b-l072z-lrwan1 working with the ping-pong application.I intend to change the example, where the board which will receive the PING will start stopped and will turn on only when a radio message is sent (in my test case, the PING).Is it p...

Resolved! stm32l476, will Different SPI busses interfere each other if one of the the SPI peripheral stops working?

I'm using stm32l476jgy6 MCU, it has 3 SPI busses, I'm using all of 3 SPI busses for different peripherals. If peripheral on SPI1 fails to communicate with MCU, will it cause any effect on other SPI busses? I've a scenario where I'm using BLUENRG-MS o...

STM BlueNRG-MS Max Characteristic length limited to 255 due to aci_gatt_add_char function limitations.

My general understanding is that the BLE standard supports characteristics with a lenght of up to 512 bytes. I'm using the BlueNRG-MS chip from STM but there the function call to add a characteristic has a uint8_t value for the length parametertBleSt...

aj.sk by Associate III
  • 3887 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.