2019-04-16 6:24 AM
Greetings, I'm configuring the S2-LP to act as a receiver and then strobing the reception. Sometimes the reception works and the S2-LP goes to the RX state as seen from the first 2 bytes of status on MISO . Sometime, randomly, it goes into an unknown state of 0x14 (MC_STATE0 value is 0x29). Why does this happen?
I don't know what other info is needed, please let me know and I'll answer.
Regards, Prithvi
2020-03-17 1:35 AM
Hi,
I am having a similar issue, but just with MC_STATE0=0x74 instead.
Did you ever find out why or how to solve it?
My question is here:
https://community.st.com/s/question/0D53W000002eTkjSAE/my-s2lp-tranceiver-is-reporting-state-0x74
Kind rgds
Anders
2020-03-17 8:54 AM
Hi again
I found out that I needed this in my mode-switch in order to re-calibrate the RCO:
S2LPRefreshStatus(); // g_sStatus_MC_STATE
// Recovery
if (g_xStatus.MC_STATE != MC_STATE_READY && g_xStatus.MC_STATE != MC_STATE_TX && g_xStatus.MC_STATE != MC_STATE_RX && g_xStatus.MC_STATE != MC_STATE_STANDBY && g_xStatus.MC_STATE != MC_STATE_SLEEP)
{
printf("S2LP Recovery...\r\n");
S2LPCmdStrobeSabort();
HAL_Delay(1);
S2LPCmdStrobeStandby();
HAL_Delay(1);
S2LPCmdStrobeReady();
HAL_Delay(1);
}I actually force it using S2LPCmdStrobeLockTx(); in the init() followed by S2LPCmdStrobeSabort(); but I still get MC_STATE=0x74 or sometimes 0x14.
Someone mentioned that there is an ERRATA sheet where something about callibration word is mentioned and how to fix it. It is not it the S2-LP Errata sheet section but I would like to know where?
Kind regards
Anders Dam Kofoed
DataHamster.io
2021-04-26 1:34 AM
I have observed as well the LP-SP2 going to the STATE 0x14 (MC_STATE0 = 0x29) with the following differences:
1- It happens now and then at very low tempertares: -34°C and then also out of specified range, at -50°C
2- it happens when I send the SABORT strobe to bring the chip from RX to READY state.
Once the LP-S2 is in the STATE 0x14 (MC_STATE0 = 0x29), how can I bring the LP-SP2 from this undocumented state to the READY state?
I have tried sending SABORT and also the READY strobes. None of them did "the magic". :(
I have contacted STMicro. If I get some information I will post it.
Marcos
2021-04-26 2:19 AM
Looking forward to your reply.
If we are to make production-ready code for the S2LP, then we must have ST to help with this - supplying us with a workaround!
2021-05-03 6:15 AM
hello, my s2lp goes to unknown state too, i couldnt reproduce the bug, do you know the difference between state LOCKON and LOCK_ST ?
2021-05-03 6:34 AM
After analysing, modifying and testing the fix I must correct my post written 7 days ago. In that post is to be read:
2- it happens when I send the SABORT strobe to bring the chip from RX to READY state.
It is the SABORT command that makes it actually possible to bring the LP-S2 from the undocumented state 0x14 (MC_STATE0 = 0x29) to the READY state.
2021-05-03 8:30 AM
Did you ever receive a reply from ST?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.